Shuweihat combined cycle power plant
09/01/2005 | The photo shows the Shuweihat combined cycle power plant (CCPP) in the United Arab Emirates. The multi-shaft plant is equipped with five SGT5-4000F gas turbines, two steam turbines and two air cooled generators. The capacity of the plant is 1500 megawatts. The sea water desalination unit supplied with steam from the combined cycle process has a water output of 100 MiGD (million imperial gallons per day).