San Pedro de Macorís combined cycle power plant
01/01/2003 | The photo shows the three units of the San Pedro de Macoris combined cycle power plant (CCPP) in the Dominican Republic. The single-shaft plant is equipped with SGT-1000F gas turbines, air cooled generators and the SPPA-T2000 instrumentation and control system. The capacity of the plant is 300 megawatts.