Hochspannungs-Gleichstrom-Übertragungsprojekt „BritNed“
06/01/2007 | Siemens Power Transmission and Distribution (PTD) and Dutch consortium partner BAM Civiel to supply the converter stations for the BritNed interconnector project. The 260 kilometers long HVDC submarine cable link between the Isle of Grain in Kent, southeast England, and Maasvlakte near Rotterdam will allow power transmission of 1000 MW at a DC transmission voltage of 450 kV as from late 2010.