Skip to Content

http://www.siemens.com

Skip over Language Selection

Change language to

Skip over Primary Navigation

Primary Navigation

Skip over secondary navigation

Secondary navigation

Skip over Site Map & Contact

Site Map & Contact

Skip over Search


Content Visual

Content
Siemens to supply two HVDC converter stations for the Danish Storebælt Project

Siemens to supply two HVDC converter stations for the Danish Storebælt Project

05/14/2007 | As part of Denmark’s Storebaelt power transmission project, Siemens is constructing both converter stations for the high-voltage direct-current (HVDC) route between the islands of Funen and Zealand. The 400-kV connection with a power rating of 600 MW will link the Western with the Eastern Grid. This will increase the reliability of the Danish power supply by enabling the exchange of electrical energy with other parts of the country via the new power link.

 
 
Downloads

Footer

Context Zone

Dialogue & Service

Service & Support


Related informations