Skip to Content

http://www.siemens.com

Skip over Language Selection

Change language to

Skip over Primary Navigation

Primary Navigation

Skip over secondary navigation

Secondary navigation

Skip over Site Map & Contact

Site Map & Contact

Skip over Search


Content Visual

Content

For the trade press


Static Var Compensator from Siemens stabilizes high-voltage transmission network in Denmark

Erlangen, Germany, September 20, 2007

The Static Var Compensator (SVC) built by Siemens Power Transmission and Distribution (PTD) in Radsted on the island of Lolland on behalf of the largest Danish consumer owned power company, SEAS-NVE, went into operation in summer 2007. The main reason to integrate the compensator in the network was voltage fluctuations caused by the 165.5 MW Nysted offshore wind park connected to the offshore platform, also operated by SEAS-NVE, which affected the voltage quality in the 132-kV transmission network. The Siemens system provides the reactive power needed for this, improves the voltage quality and increases the system stability of the weak transmission grid in the south of Denmark. It will also help minimizing any impact on the transmission system in the future that results from further wind farms planned in this region.

The main element of the Danish turnkey project is the Static Var Compensator for the 132 kV transmission system in the Radsted high-voltage switchgear station on the island of Lolland. This also includes the expansion of the existing 132 kV outdoor switchgear station for linking the SVC to the power grid. Siemens developed an advanced, innovative solution for Radsted that met the requirements of the power company while also complying with the extremely high standards for noise abatement. The SVC system operates in a twelve-pulse configuration consisting of a thyristor-controlled reactor (TCR) and one filter in each of the two secondary circuits of the high-voltage transformer. The twelve-pulse configuration has the advantage that the odd-order harmonics which are generated by each of the TCR branches mutually compensate each other. This configuration thus helps the system fulfill the strict requirements in terms of maximum occurrence of undesired harmonics at the system connection point.

 

In order to meet the rigid audible noise requirements that apply in the vicinity of the system, the SVC has been enclosed completely inside a building for the first time and has been equipped with special noise deadening materials and components. Since the height of the building must not exceed six meters, Siemens optimized the equipment configuration of the SVC accordingly.

 

Static Var Compensation is a part of the FACTS technology (Flexible Alternating Current Transmission Systems). FACTS can control the parameters that determine the operation of the power grid and define for the quality of transmission. These parameters include transmission impedances, currents, voltages and phase angles between the different network nodes. A distinction is made in reactive power compensation between parallel and series compensation. Series compensators connect capacitors – if necessary in combination with controllable reactors (TCR) – into the high-voltage transmission line. This fixed or variable reactive impedance reduces the transmission angle so that greater active power can be transmitted without jeopardizing the stability of the system.

 

In the case of parallel compensation, a variable reactive power source feeds into a selected network point via a transformer. The reactive power needed in each case is generated there in order to keep the voltage at a constant level. The system voltage can be exposed to undesired fluctuations due to load shut off or power system faults, such as short-circuits, which need to be controlled quickly. As in the Radsted substation, this function is performed by a Static Var Compensator within its power range, which is designed to match the particular network.

 
 

The Siemens Power Transmission and Distribution Group (PTD), headquartered in Erlangen, Germany, is one of the leading global players in its market sector. As a product supplier, system integrator, solution designer and service provider, Siemens PTD ensures - for utilities and industry alike - the efficient and reliable transmission of electrical energy from the power plant to the consumer. With a worldwide workforce of about 27,500 and operations in more than 100 countries, PTD had sales of 6.5 billion euros according to U.S. GAAP in fiscal 2006. Further information at www.siemens.com/ptd.

Reference Number: PTD H 200709.473 e

Press Contact

Dietrich Biester 
P.O. Box 3220
91050 Erlangen

Phone: +49-9131-7-33559

Fax: -33615

dietrich.biester@siemens.com


Footer

Context Zone

Dialogue & Service

Service & Support


Related informations