Hoher Wirkungsgrad Hohe Verfügbarkeit Hohe Flexibilität Niedrige Emissionen High efficiency High availability High flexibility Low emissions

Skip to Content

http://www.siemens.com

Skip over Language Selection

Change language to

Skip over Primary Navigation

Primary Navigation

Skip over secondary navigation

Secondary navigation

Skip over Site Map & Contact

Site Map & Contact

Skip over Search


Content Visual

Content

For the trade press


Siemens commissions another high voltage DC transmission system in China – 3000 MW carried at low loss over 1225 kilometers to Guangdong

Erlangen, Germany, February 19, 2008

After successful completion of the test phase, Siemens Energy commissioned the “Guizhou-Guangdong II” high voltage DC transmission link (HVDC) on schedule at the beginning of January. 3000 MW of electric power now flows from hydroelectric and coal-fired power plants in western China over 1225 kilometers (760 miles) to the urban and industrial centers of Guangdong province at a DC transmission voltage of +/- 500 kV. Siemens built the system together with Chinese partners on behalf of the China Southern Power Grid Company, a state-owned energy power supply company in Guangzhou. The value of the order for Siemens was over EUR100 million.

The burgeoning demand for power in China’s urban and industrial centers requires the transmission of large amounts of energy over distances of several hundred miles or more. This is only technically feasible and economically viable using high voltage DC transmission. China has increased the DC transmission voltage of future large-scale HVDC transmission links to +/- 800 kV, since China’s demand for power is growing and with it the need for longer power transmission routes.

 

“In this time of tremendous economic growth in China, our innovative high voltage DC transmission technology is not only facilitating the efficient, environmentally friendly use of energy sources located far from centers of consumption. With our solutions, we’re also helping to build reliable, sustainable energy systems in this very populous country,” said Dr. Udo Niehage, CEO of the Power Transmission Division of the Siemens Energy Sector.

 

Siemens is one of the global technology leaders in the field of high voltage DC transmission. At present the company is building an HVDC transmission system between the province of Yunnan in the south west of China and the southern province of Guangdong together with Chinese partners, again for the China Southern Power Grid Company, Guangzhou. This system will be the first in the world to transmit 5000 MW of electrical power at a DC transmission voltage of +/- 800 kV. Siemens’ share of the order volume amounts to more than EUR300 million. The system is scheduled to go into operation by mid-2010.

 

This 800-kV long-distance link is the fifth Siemens HVDC transmission project in China. The first was the “Ge-Sha” HVDC transmission link between Gezhouba and Shanghai (1200 MW, +/-500 kV over 1040 km or 645 miles). This system has been in operation since 1989. The second project “Tian-Guang” was implemented between Tianshengqiao in the south west of the country and Guangzhou (1800 MW, +/- 500 kV over 960 km or 600 miles) and has been in operation since June 2001. The third system “Guizhou-Guangdong I” between Anshun in the province of Guizhou and Zhaoqing in Guangdong province (3000 MW, +/- 500 kV over 940 km or 585 miles) has been transporting electrical power since the end of September 2004. Meanwhile number four, Guizhou-Guangdong II, went into service recently and is already playing its part in assuring China’s power supply.


 
 

The Siemens Energy Sector is the world’s leading supplier of a complete spectrum of products, services and solutions for the generation, transmission and distribution of power and for the extraction, conversion and transport of oil and gas. In fiscal 2007 (ended September 30, based on IFRS), the Energy Sector had revenues of approximately EUR20 billion and received new orders totaling around EUR28 billion and posted a profit of EUR1.8 billion. The Energy Sector had a work force of 73,500 at the beginning of fiscal 2008. Further information is available at: www.siemens.com/energy.

Reference Number: EPT200802.010 e

Press Contact

Dietrich Biester 
P.O. Box 3220
91050 Erlangen

Phone: +49-9131-7-33559

Fax: -33615

dietrich.biester@siemens.com


Footer

Context Zone

Dialogue & Service

Service & Support


Related informations

Guizhou-Guangdong II

After successful completion of the test phase, Siemens Energy commissioned the “Guizhou-Guangdong II” high voltage DC transmission link (HVDC) on schedule at the beginning of January. 3000 MW of electric power now flows from hydroelectric and coal-fired power plants in western China over 1225 kilometers (760 miles) to the urban and industrial centers of Guangdong province at a DC transmission voltage of +/- 500 kV.

Guizhou-Guangdong II