Hoher Wirkungsgrad Hohe Verfügbarkeit Hohe Flexibilität Niedrige Emissionen High efficiency High availability High flexibility Low emissions

Skip to Content

http://www.siemens.com

Skip over Language Selection

Change language to

Skip over Primary Navigation

Primary Navigation

Skip over secondary navigation

Secondary navigation

Skip over Site Map & Contact

Site Map & Contact

Skip over Search


Content Visual

Content

Repowering

The gas turbine (GT) in conjunction with a heat recovery steam generator (HRSG) and a steam turbine (ST), makes combined cycle power plants (CCPP) to the most efficient power generation facilities. Existing direct-fired plants can utilize this advanced cycle concept by adding a GT and a HRSG. This so-called repowering scheme makes the existing power generation facility equally efficient as modern combined cycle power plant.
There are several alternatives to combine and integrate a gas turbine into an existing steam power plant. A detailed assessment of the existing plant equipment as well as technical and economic boundary conditions of a specific project determines the optimal approach and the selection of the repowering concept. The main alternatives of repowering are illustrated in Figure 1 & 2.

 
 
Full RepoweringFull Repowering

Figure 1: Full Repowering

Full Repowering

Full repowering replaces the original boiler with a topping cycle consisting of one or more GTs and HRSGs. As the repowered cycle is similar to a modern combined cycle, this concept promises the best efficiency compared to all possible repowering schemes. It is widely used with old plants when the boiler has reached the end of its lifetime.

 
 
Parallel RepoweringParallel Repowering

Figure 2: Parallel Repowering

Parallel Repowering

In the parallel repowering concept, the original boiler will remain in operation. Additionally to the original steam source, a topping cycle will be added. Compared to the full repowering concept, this repowering scheme achieves slightly lower efficiency. Due to the two independent steam sources for the steam turbine, this concept provides a higher fuel flexibility and also greater flexibility in respect to load variations.

 
 

Footer

Context Zone

Dialogue & Service

Service & Support


Related informations